High Speed Sampled Data for WITS Analog Input Points

High speed data sampling is only available for Analog Input points, and is only available in WITS version 1.3 or later.

The WITS standard provides for high speed data sampling. This means that the Field Device may have the capability to sample and store data at a faster rate than the standard WITS periodic logging rate. Where this feature is enabled, there is a store for each analog input point. You can define the size of each store (although the size may be fixed in the device profile - see Display a WITS Device Profile). When a store is full, the Field Device will overwrite the oldest existing data. You can also specify the rate at which the Field Device will sample the analog input point.

Example:

With an analog point on a Field Device that supports WITS version 3.0, if you specify a store size of 1000 records, the Field Device will sample and store 1000 records-worth of data for that point. Once the 1000th record is reached, the Field Device with overwrite the oldest record with new data for the analog point. It will continue to store and overwrite the data in a 1000-record cycle, in order to retain the latest 1000 data records for that point.

Likewise, with an analog point on a Field Device that supports WITS version 1.3, if you specify a store size of 7 days, the Field Device will sample and store data for 7 days. After 7 days, it will start to overwrite the oldest data with new data. It will continue to store and overwrite data in a 7-day cycle, in order to hold the data for the previous 7 days.

Due to memory constraints, there may be restrictions on the number of points for which you can do high speed data sampling.

Example:

The Field Device may support high speed data sampling for:

  • All analog input points
  • A maximum number of analog input points
  • A specific list of analog input points
  • Some other combination of points.

The device profile defines the level of support for high speed data sampling (see Display a WITS Device Profile).

This high speed data sampling capability might be helpful when an unexpected system event occurs. You can then investigate the event by reading specific sampled data from around the time that the event occurred. You can:

For more information, see Retrieve Sampled Data (WITS Outstation) and see Retrieve Sampled Data (WITS Point).

When you retrieve standard logged data, Geo SCADA Expert will not retrieve sampled data as well (see Specify the WITS Properties and see Refresh (WITS Outstation)). You must specifically request the sampled data stored by the Field Device.

Use the fields within the High Speed Sampled Data section of the Input tab to specify the high speed data sampling properties.

The fields are as follows:

The two Cycle Store Size fields are mutually exclusive; the field that does not apply to the version of WITS being used will be 'grayed out' and unavailable for use.

The high speed data sampling properties may be fixed in the Field Device, so you may not be able to download changes to them. The device profile defines any fixed properties (see Display a WITS Device Profile).

 

When you have completed the point's configuration, you will need to download it to the Field Device by using the Outstation item's Download Configuration action.

If your Field Device does not support both of the following, you will need to make the same changes to the Field Device's configuration locally:


Disclaimer

Geo SCADA Expert 2021