Configure a Virtual ViewX Server Connection to the Geo SCADA Expert Server

If, as recommended, you install the Virtual ViewX server software on a separate machine to the Geo SCADA Expert server, you will need to configure a connection between both servers. This is to enable the Virtual ViewX server to access data on the Geo SCADA Expert server. You configure the connection using the Client applet. This is the same applet that you use to configure client connections in Geo SCADA Expert. The applet is installed together with the Virtual ViewX Server.

To display the Geo SCADA Expert Client applet:

  1. In Windows, select the Start menu. Scroll down the alphabetical list of installed applications and expand the EcoStruxure Geo SCADA folder.
  2. Select the Configure Connections option.
    The Client applet runs. It shows a list of the systems (Geo SCADA Expert databases) to which the Virtual ViewX server can connect (if it cannot currently connect to any systems, the list is empty). The applet includes various buttons that you can use to manage the connection configuration settings:

A User Account Control prompt may appear - select Continue on the prompt to allow the Geo SCADA Expert Client applet to run.

The Virtual ViewX System Configuration applet contains various buttons (for those buttons not mentioned here, see Display the Geo SCADA Expert Client Applet in the Geo SCADA Expert Guide to Client Administration):

Add

Use to add a system (Geo SCADA Expert database) to which the Virtual ViewX server can connect.

A Virtual ViewX server can connect to multiple systems (it can connect to a maximum of 64 servers across those systems).

A Virtual ViewX server can connect to a maximum of 4 Geo SCADA Expert servers in a single system. The number of servers to which it can connect in a single system varies, depending on the system setup. For more information, see 'Define the Node Name for a System Connection' in the topic Configure the Virtual ViewX System Connection.

Properties

This button enables you to Display the Client Configuration Window on a Virtual ViewX Server.

Remove

Use to remove a system (Geo SCADA Expert database) connection. If you remove a system , the Virtual ViewX clients are no longer able to access it.

Licenses

The Virtual ViewX server requires a single ViewX client license. This is a single license for connection to multiple systems, and can be a dongle or license file. The Geo SCADA Expert server's License Details window specifies the number of ViewX clients or Virtual ViewX clients for which it is licensed (see Understand the License Details Window on a Geo SCADA Expert Server).

Additionally, the Virtual ViewX server has to be licensed for the relevant number of Virtual ViewX client users. This is a separate software-based process from the existing Geo SCADA Expert licensing system and does not involve dongles or license files (see License your Virtual ViewX Installation).

Close

Use to close the applet.

For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.


Disclaimer

Geo SCADA Expert 2021