MaxRaw

Description

The maximum value of the raw acquired value. This property applies to analog tags.

As Geo SCADA Expert exports data that has already been scaled, additional scaling by Wonderware Historian should not be required. Therefore, Geo SCADA Expert sets the value of the ApplyScaling property to False and so this property isn't applicable.

Geo SCADA Expert Metadata Field

WH_MaxRaw

Default Value

The default value for this property is 100.

Type

Double.

Further Information

ApplyScaling

MinRaw

MaxEU

MinEU


Disclaimer

Geo SCADA Expert 2021