Configure the Time Period Shown on the X-Y-Z Plot

You can specify the time period that is shown on the X-Y-Z Plot. This defines the time period for which the X-Y-Z Plot displays trace values. You specify the time period using fields in the Time Axis Properties window (see Configure the Time-Axis Properties).

Use the Range section of the window to specify these properties:

For an example of how the above fields can be configured and used in conjunction with the Data Sampling fields, see Configure the Historic Data Resampling Settings.

These fields are displayed in place of the Offset and Interval fields when the Mode is set to 'Absolute':


Disclaimer

Geo SCADA Expert 2021