PSTN Outstations and Communications
PSTN Outstations communicate with the Geo SCADA Expert server using a dial-up modem, and are grouped into PSTN Outstation Sets.
The Geo SCADA Expert server and the PSTN outstations communicate via the Public Switched Telephone Network. This means that communications are only established under certain circumstances—in order for the outstations to report (dial in) to the Geo SCADA Expert server
With some protocols, you can associate a number of PSTN Channels with each PSTN outstation, to enable that outstation to dial out to the serve
PSTN outstations store the data from the measuring instruments and control devices to which they are attached. The data is available to the Geo SCADA Expert server upon request.
When the Geo SCADA Expert server makes a request for the logged data, it typically calls the outstation, the outstation reports the data, and then the communications line is typically closed. This type of request is called a
A similar procedure occurs when controls are sent from the Geo SCADA Expert server—the Geo SCADA Expert server calls the outstation, sends the control, retrieves any data, and then closes the line.
If required, a Queue feature can be enabled on your system to allow users to optionally queue certain pick action requests on PSTN outstations, rather than send those requests to the outstations immediately. For more information, see Define whether the Queue Parameter is Available, and see Optionally Queue Pick Action Requests on PSTN and ‘On Demand’Outstations.
PSTN communications are used when:
- A direct line connection is impractical due to the geographical location of the outstations (for example, radio communications may be impractical due to interference, or regulations regarding the erection of communication masts.)
- A direct line connection is not cost-effective (for example, it can be expensive to lay direct lines over long distances).
Additionally, outstations that usually use a permanent connection to communicate with the Geo SCADA Expert server can have a dial-up modem to use PSTN as a ‘fallback’ means of communication. Such outstations typically only use PSTN to communicate with the server if Geo SCADA Expert detects that the direct channel or channels via which they normally communicate have failed. Once permanent communications is re-established, the outstations return to using the direct channels
For an example that demonstrates how PSTN Channels might be used for inbound and outbound PSTN communications, see Define Dial In Line Properties on a PSTN Outstation.