Configuring String Points

Use Advanced EWS String Points to map text strings on Advanced EWS servers into Geo SCADA Expert.

Configure the properties of each String point using the fields on the Advanced EWS String Point Form.

This section covers configuration of the string-specific properties on the String Point tab of the Form.

Use the String Point tab to:

Properties on other tabs are common to many points, see Tabs on Point Forms in the Geo SCADA ExpertGuide to Advanced Drivers.


Disclaimer

Geo SCADA Expert 2022