Tabs on Point Forms

Point Forms have several ‘tabs’ or ‘pages’ for configuring different aspects of point data. For most points on advanced drivers, these tabs are available:

Identification

Use to optionally define a Help View and to indicate whether the point is to be excluded from any Exclusive Control activity (see Defining Identification Details).

Location

Use to specify the item's geographical coordinates. (You need only configure the properties on this tab if your system uses Geo SCADA Expert's Geographical Location features.)

User Methods

Use to define any custom pick actions (‘methods’) for the point (see Using the User Methods Tab to Define Custom Actions).

Alarm

Use to define optional features associated with any point alarms (see Defining an Item or Group’s Alarm Properties).

Redirection

Use to define any alarm redirections for the point (see Configure Alarm Redirections for an Item or Group).

Historic

Use to define any historic data storage settings for the point (see Defining Historic Details for a Point).

The Historic tab is only included on the relevant configuration Forms when the Historic Data feature is enabled on the server. The feature enables Geo SCADA Expert to store data historically (see Historic Data Storage Settings).

<Point Type>

Use to define any point- or driver-specific settings (see Processing Alarm Data for Point States, and also see the driver-specific documentation).

In addition, Forms for points such as output and computed points include this tab:

Control

Use to define the control settings for a point (see the driver-specific documentation and also, as appropriate:

The control actions for a Pulse point are typically configured on the Pulse Action tab (see Defining Pulse Action Details).

Control Checks

Use to define the control checks settings for a point (see Configuring Control Checks Settings).


Disclaimer

Geo SCADA Expert 2022