Points Used on Generic Modbus Controllers
Generic Modbus controllers support a combination of these point types:
- Generic Modbus Analog Input Points—see Configuring Analog Points.
- Generic Modbus Analog Output Points—see Configuring Analog Points.
- Generic Modbus Digital Input Points—see Configuring Digital Points.
- Generic Modbus Digital Output Points—see Configuring Digital Points.
- Generic String Points—see Configuring String Points.
- Generic Time Points—see Configuring Time Points.
On the Advanced Modbus driver, Generic Time Points are currently only supported for use on the Lufkin SAMS driver. That driver is an extension of the Advanced Modbus driver.
You need to configure one point of the appropriate type per point on a controller. You configure the properties for each point using the appropriate Advanced Modbus Generic Point Form.
The rest of this section covers the configuration of properties that are common to most points supported by the Advanced Modbus driver. It includes information on how to:
- Configure Common Point Properties
- Use Persistence to Stop Fleeting Changes in Value from Changing a Point State.
For information on the minimal amount of configuration that you can undertake to produce a functional Generic Modbus point in Geo SCADA Expert, see Minimum Configuration.
In addition to the points listed above, Geo SCADA Expert can support other types of point, using an Advanced Modbus Extension Driver. For information on Advanced Modbus points not listed above, see the relevant Advanced Modbus extension driver guide.
If your system includes Generic Modbus controllers that do not have ‘live’ points, see Generic Modbus Controller and Associated Channel States.