Configuring Analog Points

In addition to the analog points mentioned below, Geo SCADA Expert can support other types of analog point using an Advanced Modbus Extension Driver. For information on any Modbus points not listed below, see the relevant Advanced Modbus driver extension guide.

The Advanced Modbus driver supports Generic Modbus Analog Input points and Analog Output points.

Configure the properties for each analog point using the fields on the Generic Modbus Analog Input Point Form, or the Generic Modbus Analog Output Point Form, as appropriate.

This section covers configuration of properties on the Analog Point tab of each Form, and the properties on the Control tab of the Generic Modbus Analog Output Point Form. For information on the fields on other tabs, see Tabs on Point Forms.

For Generic Modbus Analog Input or Analog Output points, use the Analog Point tab to:

For Generic Modbus Analog Output points there are two additional tabs: a Control Tab and a Control Checks tab.

Use the Control tab to:

You can optionally use the Control Checks tab to configure the Control Checks settings (see Configuring Control Checks Settings in the Geo SCADA Expert Guide to Core Point Configuration).


Disclaimer

Geo SCADA Expert 2022