Configuring Advanced OPC Time Points

Use an Advanced OPC Time Point to map an item within the OPC DA server to an Time point in the Geo SCADA Expertdatabase. The item needs to have a suitable data type for an time point.

Configure the properties of each Time point using the fields on the Advanced OPC Time Point Form.

This section covers configuration of the time-specific properties on the Time Point tab of the Form.

Use the Time Point tab to:

For information on the Control tab, see Define the Control Settings for a Time Point and see Update an Output Point Value on Successful Action in this driver guide.

Properties on other tabs are common to many points, see Tabs on Point Forms in the Geo SCADA ExpertGuide to Advanced Drivers.


Disclaimer

Geo SCADA Expert 2022