Retrieve Data from a Hot-Standby Radio

The configuration setup required for communicating with a hot-standby radio (also known as a dual base radio) differs slightly to that required for single radio units. It also varies, depending on the Series of Trio radios. Select the relevant entry below to display more information.

Regardless of radio Series, a hot-standby setup comprises a hot-standby controller unit that is connected to two radios that function as one base radio (a setup in which only one of the radio units is active at a time). Geo SCADA Expert communicates with the hot-standby controller unit, rather than directly with the hot-standby radio.


Disclaimer

Geo SCADA Expert 2022