Understand the Alarm Summary

The Alarm Summary displays a row of values for each alarm, and uses columns to separate and categorize the values. The column headings indicate what the values in each column represent. The columns that are displayed on the Alarm Summary can be configured by a system administrator (see Alarm Summary Display Settings in the Geo SCADA Expert Guide to Server Administration).

The default column headings for the Alarm Summary are:

 

Other columns that may be included in the Alarm Summary (depending on the setup) are:

For further fields not mentioned here, see Fields by Which you can Filter an Alarm Summary.


Disclaimer

Geo SCADA Expert 2022