Client Logging

Geo SCADA Expert includes client-side logging features that provide diagnostic data for client activity. The information included in the log files can be useful when investigating connection problems, issues with initialization, and so on.

These types of log files are available for clients:

In addition, should an exception occur on a ViewX client, exception minidump files are created (see ViewX Exception Files).

For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.


Disclaimer

Geo SCADA Expert 2022