Failed Third-Party ODBC Client - System Connections

If the third-party ODBC client - system connection cannot be established, the ODBC client will be unable to connect to Geo SCADA Expert.

The connections will fail to establish if:

The third-party ODBC client - system connection works in the same way as a ViewX - system except that it uses a different license and it requires Data Access components (to be installed on the computer that is running the third-party ODBC applications). The firewall rules for third-party ODBC client - system connections are the same as those for ViewX - system connections.

Further Information

Firewall Settings for Client - System and Server Advise Connections.

Understanding Client - System and Server Advise Connections.

Certificates for Geo SCADA Expert Server and Client Connections.

Use the Server Status Tool to ascertain the current status of server - client connections: see Server Status Information.

Enable or Disable IPv6 on the Client.


Disclaimer

Geo SCADA Expert 2022