Server Status Information

The Server Status Tool provides status information that is organized into groups of categories, each of which contains sub-categories. The Server group provides status information about the server on which you are using the Server Status Tool and it contains the following sub-categories:

NOTE: The above PCS entries appear in the Server Status Tool only if the suite of PCS prerequisite components are installed on the Geo SCADA Expert server. For more information, (see Geo SCADA Expert Prerequisite Components).


Disclaimer

Geo SCADA Expert 2022