PCS Tags

The Server branch of the Server Status Tool includes a PCS Tags category. This category provides status information about the tags that are subscribed to from the database items.

NOTE: This category only appears in the Server Status Tool if the suite of PCS prerequisite components are installed on the Geo SCADA Expert server. For more information, (see Geo SCADA Expert Prerequisite Components).

The PCS Tags category displays the following information about each tag:


Disclaimer

Geo SCADA Expert 2022