Geo SCADA Expert Prerequisite Components

Geo SCADA Expert is designed to run on a computer that has certain other components installed. The components comprise a combination of the following:
(The actual options that are offered depend on the operating system and whether any components are already installed.)

WARNING

DO NOT UNINSTALL PREREQUISITE COMPONENTS

Uninstalling the prerequisite components may result in Geo SCADA Expert being unable to provide access to certain features, or being unable to run. It could also affect system security. For these reasons, do not uninstall the prerequisite components.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

When you install Geo SCADA Expert, the components that are essential for Geo SCADA Expert to run on your operating system are installed automatically. A prompt is displayed for non-essential components, allowing you to choose the components that are relevant to your system.

We recommend that you only install components that you need for your system. For example, you only need to install the:

Installing components that are not needed on your system uses up disk space unnecessarily. It also increases the attack surface. For improved system security, you should avoid installing or running components that you do not require on your system.

Further Information

Installation of Prerequisites.

Prerequisites for machines on which Virtual ViewX is installed: see Virtual ViewX Server Prerequisite Components.


Disclaimer

Geo SCADA Expert 2022