Advises

The Advises category provides status information about the advise links between the server and clients. The server advise links enable the server to send unsolicited messages to the clients.

The status information for each server advise connection is categorized under these headings:

You should pay particular attention to the Status and Evt entries. If your system is working correctly, the Status is — and the Evt is 0.

You should also pay attention to the Backoff entry. If this shows anything other than 0, there may be abnormal network conditions that mean the server is unable to connect to the client successfully.

For more information, see Server to Client Link Problems.


Disclaimer

Geo SCADA Expert 2022