Third-Party ODBC Client - System Connections

You can use data from the Geo SCADA Expert database in third- party ODBC client applications such as SAP Crystal Reports and Microsoft Excel. The data can be used in reports, spread sheets, other databases, and so on.

To use a third- party ODBC client application to access your Geo SCADA Expert system, you need to install the Data Access components of Geo SCADA Expert on the same computer as the third- party ODBC client application(s). This is because the third- party ODBC applications need to use the Data Access components to connect to a Geo SCADA Expert database.

We refer to computers that run third- party ODBC applications and have Data Access components installed as third- party ODBC Clients.

Communications between the Geo SCADA Expert serverand the Data Access components installed on the ODBC client work in a similar way as communications between a ViewX client and Geo SCADA Expert server. The only difference is that with an ODBC client, there is a single link that is used for client to server messages and server responses. There is no server advise link for unsolicited messages from the server. For more information, Understanding Client - System and Server Advise Connections.

To allow a third- party ODBC client to access the Geo SCADA Expert system, the Data Access components have to be:

To connect a computer that runs third- party ODBC applications to the server, you can either:

Or:


Disclaimer

Geo SCADA Expert 2022