Configure the Properties on the Data Set Form
To define the properties on the Data Set Form, you need to display the Form (see Display a Form).
The Data Set Form comprises these tabs:
- Identification—Use to configure the Identification details (see Defining Identification Details).
- User Methods—Use to define any custom pick actions (‘methods’) for the Data Set (see Using the User Methods Tab to Define Custom Actions).
- Data Set—Use to specify these properties:
- Table Name—Enter a unique name for the Data Set, as you want it to appear in the Geo SCADA Expert database.
The Table Name has to begin with an alphabetical character and contain only alphanumeric characters (see Naming Restrictions). The maximum name length that you can specify is 23 characters.
Although we do not recommend its use in table names, the underscore character ( _ ) is also a legal character.
We advise that Table Names do not start with the letter ‘C’, to avoid confusion with built-in tables.
Ensure that the Table Name is not identical to that of any built-in table, other Data Set, or any other ‘custom’ tables, including Data Grids, and Historic Views.
- Title—Enter the title that is to be displayed in the header whenever operators display the Data Set’s data as a List. The Title can include character spaces.
- Table Name—Enter a unique name for the Data Set, as you want it to appear in the Geo SCADA Expert database.