Naming Restrictions

When naming or renaming an item in Geo SCADA Expert, you have to take into account these restrictions:

Further Information

Restrictions that apply to the names of Mimic Parameters: see Adding a Mimic Parameter in the Geo SCADA Expert Guide to Mimics.

Restrictions that apply to the names of parameters that you can use in Template expressions: see Template Parameters in the Geo SCADA Expert Guide to Expressions.

For examples that demonstrate using an ESCAPE clause in SQL queries, see the SQL Guide.


Disclaimer

Geo SCADA Expert 2022