Configure the Properties on the Data Grid Form

To configure the properties on the Data Grid Form, you need to display the Form (see Display a Form).

You can also display the Data Grid Form from the Queries Bar. To do this:

  1. Display the Queries Bar (see Display an Explorer Bar).
  2. Expand the Data Grids branch of the Queries Bar.
  3. Right-click on the required Data Grid entry.
    A context-sensitive menu is displayed.
  4. Select the Edit Properties option from the menu to display the Data Grid Form.


The Data Grid Form has these tabs:


Disclaimer

Geo SCADA Expert 2022