Display and Configure the Properties on the Calendar Form

Use the Calendar Form to configure the basic Calendar properties.

To display the Calendar Form and configure its properties:

  1. Display the Database Bar (see Display an Explorer Bar).
  2. Right-click on the Calendar in the Database Bar.
    A context sensitive menu is displayed.
  3. Select the Edit Properties option.
    The Calendar Form is displayed.

  4. Optionally use the Calendar Form for:
    1. Defining Identification Details.
    2. Configuring any custom pick actions that are to be associated with the Calendar (see Using the User Methods Tab to Define Custom Actions).
  5. Save the configuration.

Do not confuse ‘normal’ Calendars with Alarm Redirection Calendars that can be used to redirect alarms on a calendar basis. For information on Alarm Redirection Calendars, see the Geo SCADA Expert Guide to Alarm Redirection.


Disclaimer

Geo SCADA Expert 2022