Crystal Reports-Specific Actions
This section lists the actions that are specific to Crystal Reports. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.
You can print or export a previously generated report, using separate options in the Crystal Reports Viewer (see Using the Crystal Reports Viewer). Use those options to print or export reports that are already stored in the database, rather than ‘live’ report data.