Server Component
The Crystal Reports component is only displayed in the Installation Wizard on machines on which the Crystal Reports runtime components for the native platform are installed (see Install Crystal Reports).
You also need to install the Data Access Component on your system’s servers, along with other software. For the step-by-step procedure that you should follow in order to install the required software on your system’s server(s) and ViewX clients, see Install Crystal Reports.
For further information on installing components within the Server branch, see Install a Driver in Geo SCADA Expert in the Geo SCADA Expert Guide to Drivers.
The SAP Crystal Reports runtime components are NOT installed by default. If you intend to install them you must purchase a Crystal Reports runtime license for each server on which these components are to be operational (clients do not need a license to use the runtime components). For servers on which the runtime components are operational, the Crystal Reports runtime license is included with the Geo SCADA Expert Crystal Reports driver license. Please contact your Schneider sales representative for more information.
Geo SCADA Expert servers require the 64-bit version of the SAP Crystal Reports Runtime Engine to be selected. Geo SCADA Expert ViewX clients and Virtual ViewX servers require the 32-bit version of the SAP Crystal Reports Runtime Engine to be selected. Please select both if you are to run Server and Clients on the same computer. As the runtime components are prerequisites, you have to select them before you continue further with the Geo SCADA Expert installation (this is handled automatically in the Virtual ViewX installer). For more information about the installation order, see the Installation section of the Geo SCADA Expert Guide to the Crystal Reports Driver.
If you intend using Crystal Reports on your system, you also need to install the Crystal Reports prerequisites and driver on any