Configuring Digital Points

The DF1 driver supports multi-bit Digital Input and Digital Output points.

Configure the properties of each digital point using the fields on the DF1 Digital Point Form.

This section covers configuration of properties on the DF1 tab of the Form. Use the DF1 tab to Configure the DF1 Point Properties.

For information on the fields on the Digital Point tab, see Defining Digital Point Details in the Geo SCADA Expert Guide to Core Point Configuration.

For information on the fields on other tabs, see Tabs on Point Forms in the Geo SCADA Expert Guide to Simple Drivers.


Disclaimer

Geo SCADA Expert 2022