Tabs on Point Forms

Point Forms have several ‘tabs’ or ‘pages’ for configuring different aspects of point data. For many points on simple drivers, these tabs are available:

In addition, on drivers that support controls (outputs), a Control tab and a Control Checks tab are displayed.

For information on configuring the properties on the Control tab, see the driver-specific documentation for any driver-specific fields, and also, as appropriate:

For information on configuring the properties on the Control Checks tab, see Configuring Control Checks Settings in the Geo SCADA Expert Guide to Core Point Configuration.


Disclaimer

Geo SCADA Expert 2022