DNP3

Configure General Properties

Use the fields at the top of the Binary Point tab to define the general properties for the point. Some of these fields are common to many types of DNP3 points (see Configure General Point Properties). Properties that are specific to DNP3 Binary points are explained below:

Use the Severity field within the States section of the tab to specify the severity level(s) of alarms and events that are generated as a result of the point changing state (see Binary Point States).


Disclaimer

Geo SCADA Expert 2022