DNP3

Configure Trip and Close Pulse Actions

A Pulse (Trip-Close) has two actions. Use the fields within the Actions section of the Pulse Action tab (or the <Pulse Type> tab on some drivers) to define the properties of the Trip and Close actions.

The Severity, Description, and Confirm fields are common to pulse actions on many drivers—for information, see Define the Actions that a Pulse Undertakes in the Geo SCADA Expert Guide to Core Point Configuration. Fields that are specific to DNP3 Pulse (Trip-Close) Actions are explained below:

For an illustrated example showing how On Time and Off Time parameters can be used, see Pulse Control Example.


Disclaimer

Geo SCADA Expert 2022