DNP3

Define Whether the Slave Outstation Logs Authentication and Key Change Information

The Slave outstation (Geo SCADA Expert) can log information about both successful and unsuccessful authentications and Session Key Changes. (To help protect against ‘denial of service’ attacks, the Slave outstation (Geo SCADA Expert) will transmit only a limited number of error messages before ceasing to send such messages (see Specify the Maximum Error Count).)

Use the field(s) within the Alarm/Event Logging section of the DNP3 Slave Outstation Form’s Security tab to define the priority that Geo SCADA Expert assigns to the authentication and key change information that it logs for this Slave outstation.


Disclaimer

Geo SCADA Expert 2022