DNP3

Specify the Maximum Error Count

Geo SCADA Expert can detect errors during any part of the authentication process, including challenge-responses, Aggressive Mode requests, Aggressive Mode confirmations, and Session Key Changes. If Geo SCADA Expert detects an error during the authentication process, it will determine whether it needs to report that error to the outstation. For example, if Geo SCADA Expert received a critical response from an outstation, it issues a challenge to that outstation and waits for a response. If the outstation does not respond, or responds with an incorrect reply, Geo SCADA Expert may generate an error message.

A malicious user may use a device to mount a denial-of-service attack against Geo SCADA Expert by repeatedly sending ‘bad’ authentication messages. They may also send repeated challenges in an attempt to learn about Geo SCADA Expert’s authentication. The Maximum Error Count setting helps to protect against such attacks by stopping Geo SCADA Expert from transmitting error messages once a defined limit has been exceeded. This is in accordance with the DNP3 standard.

Maximum Error Count

Use the Maximum Error Count spin box on the Security tab to specify the maximum number of authentication error messages that Geo SCADA Expert is to send to this outstation:

You can specify a maximum error count of between 0 and 10 inclusive (with 2 being the default). Once this count has been exceeded, Geo SCADA Expert will no longer send authentication error messages to this outstation.

The error count resets when either of the following occur:

If the error count is exceeded in Geo SCADA Expert for any reason, Geo SCADA Expert will initiate a Session Key Change.

If the error count is exceeded during a Session Key Change, Geo SCADA Expert will assume that the outstation does not support DNP3 Secure Authentication, or does not have DNP3 Secure Authentication enabled. Further communications will proceed without any authentication while the outstation remains online. (Should this occur, correct the configuration in the relevant device so that there is no longer a security mismatch.)

Further Information

Define Whether Geo SCADA Expert Logs Authentication and Key Change Information.

Aggressive Mode: see Specify Whether Aggressive Mode is Used.


Disclaimer

Geo SCADA Expert 2022