Reset Download Required Flags

Associated with: DNP3 SACADAPack E outstations and DNP3 SCADAPack Remote E outstations.

Security permission required to access this pick action: Configure.

Use the Reset Download Required Flags pick action to instruct Geo SCADA Expert to clear Configuration Change and Download Required for the outstation, so that the outstation is no longer flagged in Geo SCADA Expert as requiring configuration. Also, if you select this pick action, Geo SCADA Expert will not download existing configuration changes to the outstation if a Geo SCADA Expert operator chooses the Download Configuration pick action with the Changed Configuration Only option set. See Downloading Configuration Changes.


Disclaimer

Geo SCADA Expert 2022