Alarm Conditions Section
            In the Database Schema, the Alarm Conditions section shows information about the Alarm Conditions of the class.
Example:
The Alarm Conditions section for the CPointAlg class shows information about the alarm conditions that are available to analog points.
                        
                    
For each Alarm Condition of the class, the following information is shown:
- Name—The name of the alarm condition. This indicates the type of alarm.
 - Category—Indicates the category for the alarm condition. The category is used internally to group alarm conditions according to their type. In effect, the category acts as a description of the type of alarm that the alarm condition represents.
			
Example:
The alarm condition named Digital has a category of Point State. This indicates that the Digital alarm condition relates to the state of a digital point.
 - Sub Conditions—Displays the conditions that can cause the alarm to be raised.
 
As the Alarm Conditions are of the CAlarm class, they also provide access to the Fields and Methods for the CAlarm class.