Enable Comms Logging

Associated with: Channels

Security permission required to access this pick action: Diagnostics

Use this pick action to log the ‘good’ communications on a channel (see Enable or Disable 'Normal' Communications Logging on a Channel in the Geo SCADA Expert Guide to Server Administration).

Comms Logging on a channel is not enabled by default. Before enabling such logging, ensure that enough disk space is available to store the log files that will be produced.

The Logging system color indicates that Communications, I/O Logging, or Telnet monitoring are enabled on a channel. The Comms Logging status attribute indicates the channel’s current Comms Logging status.

For more information, see Communications Logging in the Geo SCADA Expert Guide to Server Administration.

If using this pick action with the Automation Interface, you need to specify the method name EnableLogging.

Also see Disable Comms Logging.


Disclaimer

Geo SCADA Expert 2022