Enable Controls
Associated with: Output points and pulse actions
Use this pick action to allow presently inhibited control actions to become available for selection on a point or pulse action.
The Enable Controls pick action is only available on a point or pulse action if:
- The Disable Controls pick action has been used to prevent access to control options on that point or pulse action.
- Your User Account is allocated the Disable Controls security permission for that point or pulse action.
Also see Control, and see Inching.