Enable IO Logging
Associated with: Channels on advanced drivers
Security permission required to access this pick action: Diagnostics
Use this pick action to enable I/O logging on a channel. When enabled, Geo SCADA Expert logs the communications that occur on the channel, including any data that is discarded by the driver (see Enable or Disable I/O Logging on a Channel in the Geo SCADA Expert Guide to Server Administration).
IO Logging on a channel (not to be confused with the I/O logging option on a driver) is not enabled by default. Before enabling such logging, ensure that enough disk space is available to store the log files that will be produced.
The Logging system color indicates that Communications, I/O logging, or Telnet monitoring are enabled on a channel. The IO Logging status attribute indicates the channel’s current I/O Logging status.
For more information, see Communications Logging in the Geo SCADA Expert Guide to Server Administration.