ApplyScaling

Description

This value indicates whether the historian applies scaling to the analog tag. The historian scales raw values to engineering units by using linear interpolation between the end points. As Geo SCADA Expert exports data that has already been scaled, additional scaling by the historian should not be required. If the value for this property is set to True, then the historian in the AVEVA application applies scaling. Therefore, the value for this property should be set to False.

Geo SCADA Expert Metadata Field

WH_ApplyScaling

Default Value

The default value for the property is False.

Type

Boolean.

Further Information

MaxEU.

MinEU.

MaxRaw.

MinRaw.


Disclaimer

Geo SCADA Expert 2022