MinRaw

Description

The minimum value of the raw acquired value. This property applies to analog tags.

As Geo SCADA Expert exports data that has already been scaled, additional scaling by the historian should not be required. Therefore, Geo SCADA Expert sets the value of the ApplyScaling property to False and so this property isn't applicable.

Geo SCADA Expert Metadata Field

WH_MinRaw

Default Value

The default value for this property is 0.

Type

Double.

Further Information

ApplyScaling.

MaxRaw.

MaxEU.

MinEU.


Disclaimer

Geo SCADA Expert 2022