Configuring ICMP Digital Points

For each network-connected device that you want Geo SCADA Expert to monitor using the ICMP driver, you need to create and configure an ICMP Digital Point in the Geo SCADA Expert database.

Each ICMP Digital Point can be in either of two states:

Configure the properties of each digital point using the fields on the ICMP Digital Point Form.

The Form has these tabs:


Disclaimer

Geo SCADA Expert 2022