Poll Statistics

Associated with: ICMP Digital Points

The Poll Statistics attribute indicates the time and date at which the Poll Times statistics were last reset.

You can reset the statistics using the Reset Poll Statistics pick action. If the poll statistics have been reset, two sets of Poll Statistics attributes are displayed. The first displays the statistics since the last reset of the poll statistics; the second displays the statistics between the previous two resets.

Example:

Since 03/Nov/2006 11:56:16.136

If the statistics have been reset, a second entry will display statistics in the form:

Between 03/Nov/2006 10:18:53.945 and 03/Nov/2006 11:56:16.136


Disclaimer

Geo SCADA Expert 2022