Group n Counter Interrogation Alarm

Associated with: IEC 60870-5 outstations

Each of these attributes indicates whether the latest Request, Freeze and/or Reset request for the counters that are assigned to that particular group, has been unsuccessful. One Group n Counter Interrogation Alarm attribute is displayed for each of the four possible counter interrogation groups.

The frequency with which Geo SCADA Expert attempts to execute the above requests is specified as part of the outstation’s configuration (see Configure the Counter Interrogation Intervals).

Possible states: Displays one of the Standard Alarm States. (Unused counter groups display the state ‘Enabled Inactive’.)

Further Information

Understand and Resolve Outstation Interrogation Alarms.


Disclaimer

Geo SCADA Expert 2022