Installing the In-Database Translation Dictionary Excel Add-In Program
The In-Database Translation Dictionary is part of the Geo SCADA Expert database and, for convenience, you can create and maintain it in a Microsoft® Excel® spreadsheet by using an Excel add-in program.
You can install the Excel add-in program on any server or client computer that meets the following recommended specifications:
You should also have Excel installed on the computer.
You can install the Excel add-in program from either:
- The Geo SCADA Expert Resource Center (if you have access to the Internet and the Resource Center webpages on the Schneider Electric Community website) or
- The Geo SCADA Expert installation disk.
To install the add-in program from the Resource Center (Geo SCADA Knowledge Base):
- In the ViewX client, select the File menu.
A context-sensitive menu is displayed. - Select the Help option.
A further context-sensitive menu is displayed.
- Select the Online Resource Center option.
The Resource Center home page is displayed in the Geo SCADA Knowledge Base area of the Schneider Electric Community website.
-
From the Child Pages list select Tools & Samples.
The Tools & Samples page is displayed.
-
Select the Software Installation Kit Link from the Excel Language/Dictionary Manager section.
The download screen is displayed.
-
Click Download to download the ExcelDictionaryInstaller.msi file.
- Open the downloaded installer file to install the Geo SCADA Expert Excel Dictionary Tool.
The Excel add-in program Setup Wizard displays.

- Follow the displayed instructions to install the add-in program.
To install the add-in program from the Geo SCADA Expert installation disk:
- Insert the Geo SCADA Expert disk. If Autorun is disabled on your PC, run the disk manually.
- When the Installer screen is displayed, select Install Geo SCADA Expert Excel Dictionary Tool.
The Excel add-in program Setup Wizard displays.

- Follow the displayed instructions to install the add-in program.