Geo SCADA Expert Server Requirements

In the following sections, we describe the recommended specifications for servers that are to run Geo SCADA Expert:

You should also refer to the following sections, which apply to both Geo SCADA Expert servers and Geo SCADA Expert clients:

Virtual ViewX is supported by Geo SCADA Expert 2019 onwards. We strongly recommend that you install the Virtual ViewX server on a different machine to the Geo SCADA Expert server. This is to avoid potential performance issues due to the number of resources that each application uses.

If you do install Geo SCADA Expert and Virtual ViewX on the same machine, both applications must have the same version and build number. This is because the applications share some resources.


Disclaimer

Geo SCADA Expert 2022