Retrieve

Use the Retrieve Excel option to load the contents of an existing In-Database Translation Dictionary into your Microsoft® Excel® spreadsheet. You can then view, update or delete the contents in Excel (see Creating and Updating an In-Database Translation Dictionary) and (see Deleting In-Database Dictionary Entries).

Follow these steps:

  1. In the Excel Geo SCADA Expert Dictionary ribbon, select Retrieve.

    Excel displays the ‘Login’ dialog:

  2. Enter your login details, as follows:
    • System Name-Enter the name of the system you want to log in to (if you have more than one system configured).
    • User Name-Enter the name of the user account you want to use.
    • Password-Enter the password associated with the user account.
  3. Select the Get Existing button.

    Excel displays the contents of the existing In-Database Translation Dictionary in your spreadsheet.


Disclaimer

Geo SCADA Expert 2022