Deleting In-Database Dictionary Entries

The In-Database Translation Dictionary is part of the Geo SCADA Expert database and, for convenience, you can create and maintain it in a Microsoft® Excel® spreadsheet by using an Excel add-in program. For more information, see Introduction to the In-Database Translation Dictionary.

To delete entries from the In-Database Translation Dictionary, follow these steps:

  1. Select Retrieve to download the contents of the dictionary to the spreadsheet (see Retrieve).

  2. Use the standard Excel features to delete the entry or entries. For more information about using standard Excel, see the Microsoft Excel Help.
  3. Select Upload and Replace (see Upload and Replace).


Disclaimer

Geo SCADA Expert 2022