Events Lists
            Geo SCADA Expert logs each activity that occurs on your system, creating an audit trail for system operation and reporting. Events are the records of the activities that have occurred on your system. Geo SCADA Expert logs events, for example, for each user interaction with the system, and for automatic system occurrences such as 
                
            
You can use either Events List to view the events and determine what has happened on your system. This is especially useful when attempting to diagnose reported faults or to determine what tasks other users have performed.
LOSS OF DATA
For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.
Refer to the following sections for details on how to use List’s common features and interpret the information that the Events Lists provide:
- Display and Use a List’s Context-Sensitive Menu
 - Displaying the Previous or Next Time Interval
 - Display a Particular Time Interval
 - Filter a List
 
Various properties affect the way in which event information is presented on a Geo SCADA Expert system. Many of these properties can be configured by system administrators and high-level engineers. Such configuration is explained in the following sections within this guide:
We strongly recommend that the Guest user account is not used for operator access. As part of this restriction, access to Queries Lists might be prohibited for the Guest User on your system. This is indicated by a diagnostic message being displayed if a user attempts to display a List such as an Events List, Historic List, or Queries List without logging on. To access such a List on a ViewX client on such a system, you have to log on using a valid User Account that has the relevant permissions and access. For more information, see Specify Whether the Guest User can Execute SQL Queries.