Add the First Instance of a Direct Variable to a Ladder Diagram

To add the first or only instance of a direct variable to a Ladder Diagram:

  1. Display the Database Bar (see Display an Explorer Bar).

  2. In the Database Bar, select the database item that represents the direct variable that you want to add to the Ladder diagram. For example, if you want to add the value of a point named 'INT 1', select the 'INT 1' point item. When you select the item, keep the left-hand mouse button pressed down.
  3. Drag and drop the database item onto the Ladder Diagram.The Add Direct Variable window is displayed.

    Use the Add Direct Variable window to define the settings for the direct variable:

    Name

    Enter the name for the direct variable. This name will be used to refer to the variable within the program. A name is entered automatically when you drag a direct variable onto the Ladder Diagram, but you can change it as required.

    Tag Type

     Choose the type of direct variable tag. This can be:

    • Read/Write (%M)—The Ladder Diagram can both read the value and overwrite it with a new value.
    • Read Only (%I)—The Ladder Diagram can only read the value and cannot change it.
    • Write Only (%Q)—The Ladder Diagram cannot read the variable but can write a new value to it.

    Tag

    This is the name of the OPC property that represents the variable that you want to add to the Ladder Diagram. The tag can be an OPC tag (for normal, direct variable values) or an OPC Historic tag (see Add Processed Historic Values to Ladder Diagrams).

    If a database item's name includes parentheses ( ), you should ensure that each opening parenthesis is paired with a closing parenthesis. If this is not the case, any Logic programs that reference the database item will not compile successfully. For example, a point named "Analog Point (4" or "Analog Point (4))" will generate a compile error message. Multiple sets of parentheses will compile successfully, including nested parentheses. For example, a Logic program can refer to a point named "Analog Point (4)" or "Analog Point (4(x))". For more information, see Limitation for Database Item Names Referenced in Logic Programs in the Geo SCADA Expert Guide to Logic.

    Type

    Choose the type of value. The value type needs to be appropriate to the value that is represented by the selected tag. For more information, please refer to Built-In Data Types.

    Insert

    Choose the type of variable tag that you are adding to the Ladder Diagram. Choose the required type of contact or coil from the combo box (see Ladder Diagram Components).

    Retained

    The Retained feature is designed to be used with internal variables. When selected, it allows the internal variable to be stored and transferred to other servers (in a multi-server setup).

    For more information on the Retain feature, see Using the RETAIN Keyword in an ST Program.

    No Cache

    Use the No Cache check box to determine whether the program uses the latest value or the initial value for a variable on each execution. If you check the No Cache check box, the program will use the latest value for the variable rather than the default value. If you clear the No Cache check box, the program will use the default value for the variable on each execution.

    The No Cache feature is especially useful with variables that are used as counts. For more information on the No Cache feature, please refer to Using VAR NOCACHE to Prevent Cached Values Being Used in an ST Program.

  4. Select the OK button to confirm.
    A direct variable tag is added to the Ladder Diagram. You can then draw connections to or from it (see Controlling the Flow of a Ladder Diagram).

If you need to add another instance of the direct variable to your Ladder Diagram, see Add Another Instance of a Direct Variable to a Ladder Diagram.


Disclaimer

Geo SCADA Expert 2022