Points Used on Lufkin SAMS Controllers
With Geo SCADA Expert’s Lufkin SAMS driver, you use:
- Generic Advanced Modbus points to retrieve current point data from a Lufkin SAMS controller. Geo SCADA Expert retrieves the data at the ‘Retrieval Interval’ specified on the Point Form (see Configure Common Point Properties in the Geo SCADA Expert Guide to the Advanced Modbus Driver).
For information on Generic Advanced Modbus points, see Points Used on Generic Modbus Controllers in the Geo SCADA Expert Guide to the Advanced Modbus Driver.
The Lufkin SAMS driver supports Generic Advanced Modbus String Points and Time Points, in addition to Generic Advanced Modbus Analog Points and Digital Points.
- Lufkin SAMS points to retrieve historic (time stamped) data that is stored on a Lufkin SAMS controller. (Lufkin SAMS points are designed to process only historic data.) Geo SCADA Expert retrieves the historic point data at the 'Historic Data Poll Interval' specified on the Lufkin SAMS outstation Form (see Define the Historic Data Poll Interval).
Lufkin SAMS controllers support a combination of these Lufkin SAMS point types:
- Lufkin SAMS Analog Input Points—see Configuring Lufkin SAMS Analog Input Points.
- Lufkin SAMS Digital Input Points—see Configuring Lufkin SAMS Digital Input Points.
For information on the minimal amount of configuration that you can undertake to produce a functional Lufkin SAMS point in Geo SCADA Expert, see Minimum Configuration.