Configure an MQTT Sparkplug™ B Device

An MQTT Sparkplug B Device represents a physical or logical device or sensor that is connected to an EoN node on an MQTT Sparkplug B Broker. The Device provides data using a compliant MQTT version 3.1.1 connection.

You configure the properties of each MQTT Sparkplug B Device using the fields on the MQTT Sparkplug B Device configuration Form. The Form has several tabs, some of which contain properties that are common to many database items, and others that contain properties that are specific to MQTT Sparkplug B Devices.

The topics in this section document the properties that are on the Device tab (see Configure the Properties on the Device Tab).

The properties on the remaining tabs are common to many database items. For information about those tabs, see Tabs that are Common to Many Configuration Forms.


Disclaimer

Geo SCADA Expert 2022