MQTT Sparkplug™ B EoN Nodes List

The MQTT Sparkplug B EoN Nodes List is specific to the MQTT Sparkplug B driver - it is only available on systems on which that driver is installed. Like other Queries Lists, you can display the List from the Queries Bar. Alternatively, you can use the Display EoN Nodes pick action to display a filtered list that just includes the EoN Nodes that reference a particular MQTT Sparkplug B Group.

The Queries List provides a summary of the status of the MQTT Sparkplug B EoN Node database items to which your User Account and the client provide access.

As with other Lists, the MQTT Sparkplug B EoN Nodes List consists of rows and columns. Each row represents an individual EoN Node and each column contains status information about that particular EoN Node item.

The MQTT Sparkplug B EoN Nodes List contains these columns:

As with other Lists, you can right-click on an entry in the List to display a context-sensitive menu. From this menu, you can select options to display further information about an MQTT Sparkplug B EoN Node, or perform various actions. For information about the actions that are specific to this type of database item, see Actions that are Specific to MQTT Sparkplug™ B EoN Nodes.


Disclaimer

Geo SCADA Expert 2022